ADC value when input is less than 0V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC value when input is less than 0V

ソリューションへジャンプ
1,731件の閲覧回数
williamely
Contributor IV

In my design I have an ADC single ended input that may experience a voltage as low as -0.1V with respect to the analog Vss. I need to know what the conversion result will be in this case.

Is it 0?

Is it undefined?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,623件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi William Ely,

It will read 0 when -0.1V connect the input pin if VSS is 0V, however I'd highly recommend that the range of the analog input voltage should within Vrefl~Vrefh.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,624件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi William Ely,

It will read 0 when -0.1V connect the input pin if VSS is 0V, however I'd highly recommend that the range of the analog input voltage should within Vrefl~Vrefh.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------