ADC on MK11

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,583件の閲覧回数
eduardrazumovsk
Contributor III

Hello,

Is there anything unique with pins ADC0_DP0, ADC0_DM0, ADC0_DP3, ADC0_DM3 ?

Is it only ADC input pins (not GPIOs) ?

Can i use those pins exactly as i meant to use the ADC0_SEx pins ?

Thanks & Regards,

Eduard

ラベル(1)
0 件の賞賛
返信
1 解決策
1,493件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Eduard,

Do you want to know how to configure the pin to ADC functions ?

If yes ,  you can see the reference manual: 10.3.1 K11 Signal Multiplexing and Pin Assignments ,

pastedImage_0.png

we can see ,  these pins "ADC0_DP0, ADC0_DM0, ADC0_DP3, ADC0_DM3" can directly be used to ADC, for these pin only have ADC function.

While , for the ADC0_SEx pins , they are multiple function , if we want to use these pin to ADC , we need configure them through  "Pin Control Register n (PORTx_PCRn) "

pastedImage_1.png

.

If i misunderstand your meaning , can you be more specific !

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,494件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Eduard,

Do you want to know how to configure the pin to ADC functions ?

If yes ,  you can see the reference manual: 10.3.1 K11 Signal Multiplexing and Pin Assignments ,

pastedImage_0.png

we can see ,  these pins "ADC0_DP0, ADC0_DM0, ADC0_DP3, ADC0_DM3" can directly be used to ADC, for these pin only have ADC function.

While , for the ADC0_SEx pins , they are multiple function , if we want to use these pin to ADC , we need configure them through  "Pin Control Register n (PORTx_PCRn) "

pastedImage_1.png

.

If i misunderstand your meaning , can you be more specific !

Best Regards,

Alice

------------------------------------------------------------------------------------------

If this post answers your question, please click the Correct Answer button.

-----------------------------------------------------------------------------------

If this post help your question, please click the helpful Answer button.

0 件の賞賛
返信
1,493件の閲覧回数
eduardrazumovsk
Contributor III

Thanks Alice

0 件の賞賛
返信