ADC on MK10DX64VLFS returs zero

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC on MK10DX64VLFS returs zero

1,170 Views
harrykoukoutos
Contributor I

On a new project with a MK10DX64VLFS, trying to read the ADC returns zero if the ADC is uncalibrated and a small value, 3-6 counts, after calibration. The same happens in internal channels, too, as the temperature sensor. Any ideas what to check? The code used is similar to the example KQRUG.pdf and to code used on a MK10DX256ZVLQ10, that works just fine. Have we missed a major difference between chips?

0 Kudos
Reply
1 Reply

1,100 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please refer the adc_demo in Kinetis 50MHz bare metal sample code(REV 1.6).

adc_demo.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply