ADC on MK10DX64VLFS returs zero

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC on MK10DX64VLFS returs zero

1,189件の閲覧回数
harrykoukoutos
Contributor I

On a new project with a MK10DX64VLFS, trying to read the ADC returns zero if the ADC is uncalibrated and a small value, 3-6 counts, after calibration. The same happens in internal channels, too, as the temperature sensor. Any ideas what to check? The code used is similar to the example KQRUG.pdf and to code used on a MK10DX256ZVLQ10, that works just fine. Have we missed a major difference between chips?

0 件の賞賛
返信
1 返信

1,119件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please refer the adc_demo in Kinetis 50MHz bare metal sample code(REV 1.6).

adc_demo.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信