ADC Problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC Problem

1,343 次查看
harshall
Contributor I

We were evaluating Freescale IC “MKM33Z128ACLH5” last from two months. But it is found that IC is not working as per expectation in its basic ADC functionality itself. For e.g. For 24 Bit ADC, it is not even showing 14 bit performance on the Freescale development board itself

0 项奖励
回复
1 回复

1,239 次查看
MarMi
NXP Employee
NXP Employee

Hello,

The peak SNR performance of the Kinetis-M SD ADC is 92dB @ PGA gain=x1, Vp-p=1V and 3000sps. It is approx. 15 bit performance - which is also the real performance=expectation of the device.

If you intend to design power meter then this SD ADC will produce very accurate results - refer to pages 25-26 of the 1 phase power meter design: http://www.nxp.com/doc/DRM143.   

For other applications, in general, you could consider software averaging but this approach will result in reduction output sample rate in turn for getting additional bits of SNR.

Kind regards,

Martin M.

0 项奖励
回复