ADC Fifo in MKE04Z64VLH4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ADC Fifo in MKE04Z64VLH4

跳至解决方案
1,199 次查看
prasannanaik
Contributor III

Hi,

   I want to sample 8 channels of ADC with single command(SW or HW trigger) without any CPU intervention.

   Is it possible to use FIFO mode of ADC for this purpose as FIFO mode offloads CPU and gives an interrupt only after sampling of all the ADC channels in ADC channels FIFO has been completed.

Also, is there any sample code that can be used for FIFO operation in MKE04Z64VLH4.

Thanks and best regards,

Prasanna

0 项奖励
回复
1 解答
1,074 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Prasanna,

Please download the FRDM-KEXX Driver Library Package (REV 2.0).
Then you will find the ADC_FIFO_demo.

ADC_FIFO_demo.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,075 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Prasanna,

Please download the FRDM-KEXX Driver Library Package (REV 2.0).
Then you will find the ADC_FIFO_demo.

ADC_FIFO_demo.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复