ADC Differential Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Differential Mode

3,631件の閲覧回数
ZYXEmbedded
Contributor I

Hi,

I enabled differential mode by setting enableDifferentialPair to true (CADC driver), and I get values between 0 and 4095.

2048  when ADC channel 0 = ADC channel 1

0 < ADC result < 2048 (when ADC channel 0 < ADC channel 1)

2048 < ADC result < 4095 (when ADC channel 0 > ADC channel 1).

 I was expecting the values to be between -4095 and 4095 (signed). The ADC result is 16 bit (3 bits left shifted and the 16th bit is signed bit when using differential mode).

Is there an example code for configuring differential mode?

I'm using MKV46 .

 

 

0 件の賞賛
返信
3 返答(返信)

3,624件の閲覧回数
D4Worker
Contributor II

Hi there, I am also using the same series. 
 
I guess the ADC register result, ADC->RSLT[0], is not producing something in the negative range. 
What I did is making a conversion function/statement to the unit / range I want. 

For your case, you are mapping (ch1-ch0) to -4095 ~ +4095 whilst the original result It 0-4095
What about a quick fix 

signed count_you_finally_get  = ((Result_original >> 3 ) << 1 ) -  4095 ?

Here >> 3 is making it right align. 
<<1 is x2 for mapping your wished range for 8192 counts. 
-4095 is the offset 

I expect there are some register setting can help manipulate the result format but I try to prevent diving into it. = )








0 件の賞賛
返信

3,605件の閲覧回数
ZYXEmbedded
Contributor I

Thank you @D4Worker,

I did something similar.

Right now I'm setting an offset of 2048, so the result is between -2048 and 2048. And then I left-shift the 13-bit result by one. I was hoping there was a way to get the values between -4095 and 4095 without performing additional operations.

 

0 件の賞賛
返信

3,583件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @ZYXEmbedded ,

This is a 12bit ADC. If the output is from -4096~+4096, that is 13bit. The signal bit is also a bit.

In fact, Differential measurements return the max value ((2**12)-1) when the + input is V REFH and the - input is VREFLO , return 0 when the + input is at V REFLO and the - input is at VREFH , and scale linearly between based on the voltage difference between the two signals.

 

Regards,

Jing

0 件の賞賛
返信