ADC+DMA+SPI for FRDM-KV31F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC+DMA+SPI for FRDM-KV31F

1,113 次查看
ray_deng1
Contributor III

Dears,

 

  We need 2 channels 1Mbps ADC conversion rate to output result via SPI, is there any example source code for this in FRDM-KV31F?

 

BRs,

Ray

0 项奖励
回复
1 回复

1,101 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ray,

The KV31 does have two ADCs which are capable of up to 1.2MSamples/second in 12bit mode. You mentioned 1Mbps, so it should be doable albeit it would also depend on the size of the samples.

There is not an SDK example with exactly this configuration, but there are some ADC and SPI examples on the FRDM-KV31F SDK which may help as a starting point.

My apologies for the inconvenience.

Regards,
Gustavo

0 项奖励
回复