ADC+DMA+SPI for FRDM-KV31F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC+DMA+SPI for FRDM-KV31F

1,037 Views
ray_deng1
Contributor III

Dears,

 

  We need 2 channels 1Mbps ADC conversion rate to output result via SPI, is there any example source code for this in FRDM-KV31F?

 

BRs,

Ray

0 Kudos
Reply
1 Reply

1,025 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ray,

The KV31 does have two ADCs which are capable of up to 1.2MSamples/second in 12bit mode. You mentioned 1Mbps, so it should be doable albeit it would also depend on the size of the samples.

There is not an SDK example with exactly this configuration, but there are some ADC and SPI examples on the FRDM-KV31F SDK which may help as a starting point.

My apologies for the inconvenience.

Regards,
Gustavo

0 Kudos
Reply