A problem with kinetis K20 IAP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A problem with kinetis K20 IAP

1,425件の閲覧回数
yuting
Contributor I

i want to wite an IAP bootloader  for K20(refer to an2295sw). I can erase program flash sector and wirte a long word into program flash sector. but if i sequentially write several long bytes. it will cause Resetting the chip. In fact, when i earase a program flash sector ,it cause resetting too.

(I operate FCCOB registers using Program Section Command and Program Longword Command)

Thanks in advance,

yuting.

タグ(3)
0 件の賞賛
返信
1 返信

1,179件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi Yuting,

Can you provide mode details about your problem?

Does the device feature FlexNVM? Which commands are you using? Program Section?
Are the flash routines executing from RAM?

Best Regards,

Alejandro

0 件の賞賛
返信