A problem with kinetis K20 IAP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

A problem with kinetis K20 IAP

986 次查看
yuting
Contributor I

i want to wite an IAP bootloader  for K20(refer to an2295sw). I can erase program flash sector and wirte a long word into program flash sector. but if i sequentially write several long bytes. it will cause Resetting the chip. In fact, when i earase a program flash sector ,it cause resetting too.

(I operate FCCOB registers using Program Section Command and Program Longword Command)

Thanks in advance,

yuting.

标记 (3)
0 项奖励
回复
1 回复

740 次查看
alejandrolozan1
NXP Employee
NXP Employee

Hi Yuting,

Can you provide mode details about your problem?

Does the device feature FlexNVM? Which commands are you using? Program Section?
Are the flash routines executing from RAM?

Best Regards,

Alejandro

0 项奖励
回复