Hi,
I got thr MKL16Z64VFT, that is a 64K flash. On the chip itself I read M16M6VFT.
Using the development SW, I can program only 32K of program.
What am I doing wrong?
Thanks
已解决! 转到解答。
Hi David R,
I already find the root problem, it is really very difficult to find it if you don't give us the project.
Your problem is not caused by the chip hardware, also not the code itself, it is caused by the debug configuration in the codewarrior.
You select the KL16Z32M4 not the KL16Z64M4, then the debug will use the 32K to debug your code, after your code larger than 32K, it will have problem.
This picture is from your debug configration: run->debug configuration
Please modify it to MKL1664M4.
After you modify it, then click ok, and debug, your problem will disappear!
Wish it helps you!
If you still have question, please contact me!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi David R,
Please follow this picture, and printf the project size information:
Then give me your project size information picture , data+bss will use the RAM size.
You should better give us your project, then we can help you to check it whether it is caused by the copy to ram function or not.
After we get your project, you can delete the attachment.
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
I really appriciate your help!! thank you!
the print of the size is below
"C:/Freescale/CW MCU v10.6/Cross_Tools/arm-none-eabi-gcc-4_7_3/bin/arm-none-eabi-size" --format=berkeley -x -t Me4_Base.elf
text data bss dec hex filename
0x7cec 0x38 0x4cc 33264 81f0 Me4_Base.elf
0x7cec 0x38 0x4cc 33264 81f0 (TOTALS)
I added the project in here and I will send you the password in email , give me your work email address.
Thanks,
David
Hi David R,
Please use the optimize to do the code optimization, then try again, I use it, then the code won't enter the interrupt.
    
You can choose the optimize level to 3, then try again on your side.
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hey ,
I don't to optimize because it is hard to debug the code , I tried to change the TSS component to GPIO method and it got better but adding some code give the same error.
I think that there is something with the TSS library , can you check it ?
Thanks,
David
Hi David R,
Did you solve your problem after follow my steps?
Any other question else?
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi David R,
I already find the root problem, it is really very difficult to find it if you don't give us the project.
Your problem is not caused by the chip hardware, also not the code itself, it is caused by the debug configuration in the codewarrior.
You select the KL16Z32M4 not the KL16Z64M4, then the debug will use the 32K to debug your code, after your code larger than 32K, it will have problem.
This picture is from your debug configration: run->debug configuration
Please modify it to MKL1664M4.
After you modify it, then click ok, and debug, your problem will disappear!
Wish it helps you!
If you still have question, please contact me!
Have a great day,
Jingjing
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi David R,
Our workflow is supporting the customer through the community with the post, the email is confidential.
Now, please follow me at first, and send me your password in the community message.
Waiting for your password.
Jingjing
Hi Santiago & Jingjing,
I added the Hard Fault handler it it seems to break in __copy_rom_section function , I tried to remove some data and still the same.
Some Questions:
1. my m_data(RAM) section start in 1FFFF800 address and has length of 0x2000 , is it correct ?
2. I tried to move to SysV and get the next data:
section size addr
.interrupts 0xc0 0x0
.cfmprotect 0x10 0x400
.text 0x7c1c 0x410
.data 0x20 0x1ffff800
.bss 0x2cc 0x1ffff820
.romp 0x18 0x1ffffaec
._user_heap_stack 0x200 0x1ffffb04
.ARM.attributes 0x31 0x0
.debug_info 0xbbc3 0x0
.debug_abbrev 0x2e33 0x0
.debug_loc 0x3316 0x0
.debug_aranges 0xbd8 0x0
.debug_macinfo 0x7e0687 0x0
.debug_line 0xad57 0x0
.debug_str 0x4756 0x0
.comment 0x79 0x0
.debug_frame 0x1fd8 0x0
Total 0x80c68a
Can I understand something from here? because my calcluation it should be fine.
I really don't understand how I got RAM full , Any Ideas?
if you have a way to check the occupied RAM I will be glad to hear it
Thanks,
David
Hello David,
Everything seems correct, the RAM is defined correctly. The Kinetis KL16 has 2 blocks of RAM:
- RAM_L: From 0x1FFF_F800 to 0x1FFF_FFFF. 2kB
- RAM_H: From 0x2000_0000 to 0x2000_1800. 6 kB
I don't understand what's going on, and without debugging it, is difficult to guess it.
What do you change to make it crash? Can you share your code?
Regards,
Santiago
Hi,
I checked a it and it handles very wierd, I wrote code for EEPROM I2C and it worked , but after I go over 32K this code stops running and throws Hard Fault ( I can see it in debugging step )
The problem is the SendBlock function, when I remove it the code is running ( same behavior with sendChar).
My code is very simple:
| CI2C1_Enable(); | |
| // set address | |
| res += CI2C1_SelectSlave(0x50); | |
| res = CI2C1_SendChar(buffer);//setting read address | 
my I2C settings ( I tried with/without Interrupt)
do you have any suggestions ?
Thanks,
David
Hello David,
As Jingjing says, I think your problem has nothing to do with the size of the code. If you can program it, the issue is not the size of the binary. Maybe you're running out of RAM memory or you're having other type of problem, but I doubt the issue is the size.
You should analyze the flow of the code and try to understand what's going on.
Regards,
Santiago
Hi David,
I think you should follow the code to check which code in SendBlock function caused the hard fault.
Please follow this post to check out which line cause the CPU enter in the hard fault.
Debugging Hard Faults on ARM Cortex-M | MCU on Eclipse
After you find the detail code, please give us the picture.
If you still not OK, please upload your project directly!
Best Regards,
Jingjing
Hello,
What development SW are you using? Have you created a new project or are you using an example? How do you know that the memory that you can program is only 32 Kb?
Regards,
Santiago
Hi,
I will answer instead of Nehemia, I am using eclipse Codewarrior 10.6. I created a new project with my controller
It worket perfectly until I go over 32KB code size , when I delete some code to be under 32K it worked again. I verifed that the text section is 64K.
Attached picture with configuration of the CPU include the text section( it is default ).
Also , When I program more than 32K if fall on PE_ISR(Cpu_Interrupt) from function __copy_rom_sections_to_ram.
Thanks,
David