3bits completely missing on the KV31 FlexBus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

3bits completely missing on the KV31 FlexBus

1,510件の閲覧回数
michaelbanak
Contributor I

FB_AD21, FB_AD22, FB_AD23, are missing in the pin out description for the  MKV31F512VL

Where did they go? FB_AD31:FB_AD24 and FB_AD20:FB_AD00 are all identified in the specification.

These three(3) bits are also missing from the config tool, yet the write-up for the FlexBus clearly calls for all 32 bits to be available.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,425件の閲覧回数
miduo
NXP Employee
NXP Employee

Hello,

Well, it seems really confused here for the FB_AD.

First, it is stated in the manual that: " FB_AD[23:21] not available on 100-LQFP devices."

And for 64 pin package, the FB_AD only to FB_AD17.

0 件の賞賛
返信