FLASHING MK60,MK66

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FLASHING MK60,MK66

2,265件の閲覧回数
durgasivakrishn
Contributor III

Hi,

I complted two projects using MK66FN2M0VLQ18 and MK60DN512VLQ10 now they are in production,

To flash my code I am using KEIL, I want to use some application to flash the devices by selecting the .hex file or .out file, is there any application to flashing the devices.

Looking forward to your reply,

Regards,

B.Durga sivakrishna

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

2,154件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

If you use Jlink to download code, you can download Segger JFlash tools. It is free. If you use P&E Multilink, Pemicro also has a tool. But it is not free. But if you use ulink/CMSIS-DAP, it seems there is no software can use it to download hex file.

Regards,

Jing

2,154件の閲覧回数
durgasivakrishn
Contributor III

Hi Jing,

Thanks for your replay, I have only ulink2.

Regards,

B.Durga sivakrishna

0 件の賞賛
返信