2x5 idc .05" cable kwikstik

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2x5 idc .05" cable kwikstik

Jump to solution
2,085 Views
mjg8t
Contributor IV

Hi there,

 

I have been working with the kwikstik and have now designed my first PCB with a k20 part onboard.  I would like to program the board uisng the j-link on the kwikstik and am looking for the easiest option to do so.  It would be optimal to use an existing 2x5 .05" pitch IDC cable and poplulate the 2x5 SWD header on the quickstik.  However I am  not finding any sources for prebuilt cables with the 2x5 female connector on both ends. 

 

Does anyone know of any resources to find such?  Or have other direct solutions?

 

Thanks.

0 Kudos
Reply
1 Solution
1,815 Views
mjg8t
Contributor IV
0 Kudos
Reply
3 Replies
1,815 Views
mjg8t
Contributor IV

FYI.  For those who might also be searching:  The closest I have been able to find are these connectors on ebay.

 

http://www.ebay.com/itm/300720309884?ssPageName=STRK:MEWAX:IT&_trksid=p3984.m1423.l2649#ht_2851wt_75...

1,815 Views
mjg8t
Contributor IV
1,816 Views
mjg8t
Contributor IV

Best yet:

 

http://www.digikey.com/scripts/DkSearch/dksus.dll?wt.z_header=search_go&lang=en&keywords=FFSD-05-D&x...

 

Or it looks like you can get samples directly from samtec.  

0 Kudos
Reply