16x2 LCD interface in FRDMK64F board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

16x2 LCD interface in FRDMK64F board

5,329 Views
titusstalin
Contributor V

Hi,

I have FRDMK64F board with me and I want to interface 16x2 LCD interface.

Could you provide some useful example code to accomplish this.

BTW, I'm using KDS as IDE.

3 Replies

2,963 Views
mjbcswitzerland
Specialist V

Hi Titus

Please see http://www.utasker.com/kinetis/FRDM-K64F.html (scroll to bottom of page)

This allows the FRDM-K64F to operate together with 1 x 8 to 4 x 40 character LCDs.

A screen shot of 2 x 16 LCD mode is shown below.

The project can be built with CW, KDS, IAR, Keil, Atollic, CooCox, Crossworks, Green Hills, GCC standalone or VisualStudio.

Regards

Mark

Kinetis: µTasker Kinetis support

K64: µTasker Kinetis FRDM-K64F support / µTasker Kinetis TWR-K64F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 Kudos
Reply

2,963 Views
BlackNight
NXP Employee
NXP Employee

Hi Titus,

I use this display: HD44780 2×16 Character Display for Kinetis and Freedom Board | MCU on Eclipse?

It is right now for CodeWarrior, but can be easily copied to KDS (see Copy of Processor Expert Components | MCU on Eclipse).

I hope this helps,

Erich

2,963 Views
juancarlossuare
Contributor III

Hi Erich.

I will use SDK 2.0, as you know this SDK has no support for Processor expert and I need a LCD 2 x 16 library (.c and .h files) in baremetal option. Do you work with baremetal code?

0 Kudos
Reply