12 bit DAC in k40 Series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

12 bit DAC in k40 Series

Jump to solution
7,241 Views
mf_kappa
Contributor II

Hi

I'm using the DAC in "non buffer" mode, SW trigger

1. What is the SW trigger for the DAC to start convert form digital to analog? Is it the write to DATA registers ? (high register or low register ?)

2. What bit tell me that the conversion is completed, and I can convert new data?

3. If I configure the two DAC's in my MCU (DAC0, DAC1) to start convert, is the data converted in parallel?

Thanks

Labels (1)
Tags (1)
1 Solution
5,687 Views
mjbcswitzerland
Specialist V

Hi

1. When the SW mode is selcted (DACTRGSET set) a write to DAT0 triggers the conversion. The Freescale examples write DATL followed by DATH but I found that a single half-word write has the same effect and is of course more efficient.

2. There is no status bit showing the status of the conversion. The delay between triggering the new value and the output settling to its final value depends on the size of the voltage change and also whether the low power or high power operation is set - the high power mode is about 7x faster. Since the output change is a "settling time" rather than a conversion as such (a bit like charging a capacitor to the new value) the speed of writing should be done in accordance to the worst case settling charge - if faster, it will result in a low-pass filter action since the output can't get to the intermediate value. Triggering from a timer is probably the best method if writing continually at a fast rate - it is also important to have an accurate base clock in case of generating specific waveforms.

3. DAC0 and DAC1 are independent and so work in parallel.

Regards

Mark

http://www.uTasker.com

View solution in original post

0 Kudos
Reply
7 Replies
5,687 Views
franciscofernan
Contributor II

Hi mf_kappa,
Because this post is a few years old i'm not sure if i should be asking this question here.
Basically for the past month I've been learning embedded programming while working with TWR-K40X256 (MK40DX256ZVMD10 micro-controller). Right now I'm tasked with converting a generic sinusoidal wave (like a sum of sines) via ADC, applying some basic digital signal processing to the data and then converting the processed digital data back to analog using DAC (kinda similar to yours if i understood correctly).
I've decided to use Processor Expert for this and so I've added the components DAC_LDD and ADC_LDD to the project (images of the configurations below).
Looking through the Typical Usage for both the components I've tried to implement a continuous measurement of a selected sample group (w/ interrupt service) without much success (measured values are always 0) and for the DAC part i am generally not sure about the way to implement the conversion.
Do you have some suggestions or code snippets on how to solve the problem/implement the system I explained?
I'm sure this is a basic work and all these doubts must be born on my inexperience.

Thank you for all the attention!

DAC_config.pngADC_config.png

0 Kudos
Reply
5,687 Views
mjbcswitzerland
Specialist V

Hi Francisco

I can't help with the PE setup but if you want a working solution you can simply use the uTaskerV1.4 project which includes a buffered ADC/DAC configuration based on DMA and PDB which is very practical for adding signal processing in between.

The ADC/DAC configuration and operatrion is explained in the document http://www.utasker.com/docs/uTasker/uTaskerADC.pdf

Download the uTasker project from http://www.utasker.com/forum/index.php?topic=1721.0 - it will build with CW, KDS, IAR, Keil, Rowley, Atollic, Coo Cox, standalone GCC or Visual Studio. Then select your processor and board in config.h:

#define KINETIS_K40 // choose family

#define TWR_K40X256 // choose board

In app_hw_kinetis.h enable both ADC and DAC support: #define SUPPORT_ADC and #define SUPPORT_DAC

In ADC_Timers.h enable the ADC/DAC operation with #define TEST_AD_DA and make any configuration changes according to the interfaces in the document (sampling rate, resolution, buffer size, DMA channel allocation etc.)

On each half-buffer completion there is an event ADC_TRIGGER_1 (see handling in ADC_Timers.h) and code there can process the buffer as required - it has to be complete before the next half buffer is required so adjusting the buffer size allows compromising between buffer processing rate and delay.

Regards

Mark

µTasker Kinetis support

5,686 Views
mjbcswitzerland
Specialist V

Hi

As reference I have built the project for the K40 tower board (with settings as above) and attached it as binary file. The potentiometer voltage (on ADC input ADC_DM1_SINGLE) is passed to the DAC0 output (A32 on the primary back plane connector) after a 1s delay.

In addition it will drive the SLCD module with the time (RTC) and there is a command line menu on the serial connector (115200Baud).

Regards

Mark

0 Kudos
Reply
5,688 Views
mjbcswitzerland
Specialist V

Hi

1. When the SW mode is selcted (DACTRGSET set) a write to DAT0 triggers the conversion. The Freescale examples write DATL followed by DATH but I found that a single half-word write has the same effect and is of course more efficient.

2. There is no status bit showing the status of the conversion. The delay between triggering the new value and the output settling to its final value depends on the size of the voltage change and also whether the low power or high power operation is set - the high power mode is about 7x faster. Since the output change is a "settling time" rather than a conversion as such (a bit like charging a capacitor to the new value) the speed of writing should be done in accordance to the worst case settling charge - if faster, it will result in a low-pass filter action since the output can't get to the intermediate value. Triggering from a timer is probably the best method if writing continually at a fast rate - it is also important to have an accurate base clock in case of generating specific waveforms.

3. DAC0 and DAC1 are independent and so work in parallel.

Regards

Mark

http://www.uTasker.com

0 Kudos
Reply
5,686 Views
mf_kappa
Contributor II

Hi Mark

Thanks for your answer !

I still have a question regards the DAC:

You recomended to trigger the DAC from a timer. In my application, I need to wait a ADC conversion

before triggering the DAC. (The basic flow of this application is: sampling data via ADC, then perform math operations of the digital sampling, Finally, convert the digital data to analog using DAC)

My application need to work very fast rate.

Do you reccomend to trigger the ADC and the DAC using the same timer?

Or trigger only the ADC by timer and trigger the DAC by SW (wait until ADC finish sampling)?

Regards

0 Kudos
Reply
5,686 Views
mjbcswitzerland
Specialist V

Hi

That is a design question which may have several different possible answers.

Since I haven't used the buffered mode (yet) I don't know all details but I known that the timer modules can be used to tigger DAC conversions (with up to15 buffered output values in a queue). DMA is possible and it is also possible to trigger the DAC from the ADC.

Since you need to process the ADC value before sending it to the DAC it may be interesting to use the buffer as short delay line - ADC and DAC triggered essentially from the same timer but the buffers used to allow some jitter in the SW time from the ADC inputs to the DAC outputs. As long as the buffer doesn't completely empty the SW just has to ensure that there is at least one sample ready when needed. Whether you can affort a few samples of delay depends on the exact requirements but it may be better than having jitter on the exact output sample time due to SW jitter between the ADC input sample completion and the DAC write.

Regards

Mark

http://www.uTasker.com

5,686 Views
mf_kappa
Contributor II

Hi Mark

Thanks you very much for your answers, again !

0 Kudos
Reply