unkown type error when using KSDK along with PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

unkown type error when using KSDK along with PE

1,274件の閲覧回数
hanchengyang
Contributor II

Hello,

 

I created a project using KSDK/PE with MQX, 1 task added, 1 event created, but when compiling:

22422_22422.pngQQ截图20150422112442.png

when i go into psp_time.h, and right click PSP_TICK_STRUCT_PTR to open declaration, KDS can find the declaration in the mqx.h.

So it's the problem of compiler settings?

 

Find my project in attach

 

Thanks,

Hancheng YANG

Original Attachment has been moved to: 2204_migration_KSDK_PE_d.7z.zip

ラベル(1)
0 件の賞賛
返信
1 返信

1,168件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

When  use MQX_KSDK,  it needn't add the mqx_ksdk component,  we  only need choose here :

17978_17978.pngpastedImage_0.png

this function is equivalent to MQX_KSDK.  There are all the OS the KSDK concluded, we can refer to our need select.

Please see the attachment , it is a project i create on my side , you can try it on your side .


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信