unkown type error when using KSDK along with PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unkown type error when using KSDK along with PE

1,295 Views
hanchengyang
Contributor II

Hello,

 

I created a project using KSDK/PE with MQX, 1 task added, 1 event created, but when compiling:

22422_22422.pngQQ截图20150422112442.png

when i go into psp_time.h, and right click PSP_TICK_STRUCT_PTR to open declaration, KDS can find the declaration in the mqx.h.

So it's the problem of compiler settings?

 

Find my project in attach

 

Thanks,

Hancheng YANG

Original Attachment has been moved to: 2204_migration_KSDK_PE_d.7z.zip

Labels (1)
0 Kudos
Reply
1 Reply

1,189 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

When  use MQX_KSDK,  it needn't add the mqx_ksdk component,  we  only need choose here :

17978_17978.pngpastedImage_0.png

this function is equivalent to MQX_KSDK.  There are all the OS the KSDK concluded, we can refer to our need select.

Please see the attachment , it is a project i create on my side , you can try it on your side .


Have a great day,

Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply