rebuilding after component change

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

rebuilding after component change

869 次查看
kevinhalberg
Contributor II

I am using KDS v3.0.0 and have been using PE a lot for all the peripherals on a K65 uC.  I find sometimes that when I change a setting a save it that it doesn't always rebuild.  I found changing the baud rate in my UART component especially prone to this.  Is there a way to force KDS to tell PE that something changed and have it rebuild so that the changes are reflected in the Generated_Code?

 

Thank you,
Kevin

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

790 次查看
BlackNight
NXP Employee
NXP Employee

Hi Kevin,

I have not seen something like this.

if you change a setting, and you generate code, and it does not build the changed files, then this would be a bug.

Could you report other details? Have you generated code?

Note that there is a setting to disable code generation (see How to Avoid Slow Processor Expert Projects | MCU on Eclipse ) in case you want to do it manually. Maybe you have enabled that setting, and code is not generated after you have changed something?

Thanks,

Erich

0 项奖励
回复

790 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kevin,

After you change the code , if you do not want the PE change the code you write , you can select ""Don't Write Generated Component Modules"

pastedImage_0.png

thus , when rebuild the project , the code you write won't disappeared .

Hope it helps

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Have a great day,
Alice

0 项奖励
回复