rebuild toolchain for kinetis from scracth

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

rebuild toolchain for kinetis from scracth

1,951 次查看
mastupristi
Senior Contributor I

I need to rebuild whole kinetis toolchain from scratch.

 

I need to start from source code, applying patches, configure and build. In other words I need to replicate exactly the steps followed by Freescale to build toolchail delivered with KDS 3.0.0

Where can I find detailed instructions?

 

I mean: where to find source code, patches and other stuff? How to configure?

 

best regards

 

max

标签 (1)
0 项奖励
回复
4 回复数

1,740 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hello max

please log on NXP web site then go to this url

Kinetis Design Studio Integrated Development |NXP

then follow attached video to get the KDS 3.0 installer and all updates

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,740 次查看
mastupristi
Senior Contributor I

No, it doesn't help.

I have already downloaded and installed KDS 3.0.0.

I need to rebuild toolchain eg. for 64 bit systems, so the first step is to find source code and patches to apply, then configure and compile.

best regards

0 项奖励
回复

1,740 次查看
BlackNight
NXP Employee
NXP Employee

Hi Max,

KDS V3.0.0 uses stock launchpad (GCC ARM Embedded in Launchpad ) GNU build tools, without modifications. You should be able to re-build it yourself with the information and sources available from the Launchpad site.

I hope this helps,

Erich

0 项奖励
回复

1,740 次查看
pgo
Senior Contributor V

Hi Max,

I'm uncertain if this is what you are after but the toolchain included with KDS is a (I hope lightly) modified version of the Open source toolchain:

https://launchpad.net/gcc-arm-embedded

Source code and such is available via the above link.

bye

0 项奖励
回复