program MK22FX512VLK12 with MK22FN512VLK12 Freedom Board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

program MK22FX512VLK12 with MK22FN512VLK12 Freedom Board

跳至解决方案
1,057 次查看
jacewalton
Contributor III

I have the freedom board containing the MK22FN512VLK12 chip set  and was told that this board can be used to program the MK22FX512VLK12 chip set. (there are slight differences between the chips how can that be done? Through JTAG I assume. Has anyone done this? I would like to save $200 on a P&E programmer. 

using Kenitis IDE v 3.0

thanks!

标签 (1)
1 解答
858 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jace,

I recommend you refer to this tutorial :

Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse 

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
859 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Jace,

I recommend you refer to this tutorial :

Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse 

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------