problem with segger debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem with segger debugger

2,254 Views
zohargolan
Contributor III

hi all,

 

I am trying to debug a custom board using KDS 3.0.0 and a segger j-Link ultra+. The board have a Kinetis mk20dn512 device connected in a jtag chain with altera device.

I don't have an hardware problem since I can use PE-Micro debugger in this configuration, and I also can use the segger debugger on this board if I am using the IDE from IAR.

The problem is when I am trying to open the debugger I am getting the following error log

 

 

SEGGER J-Link GDB Server V5.10c Command Line Version

 

 

 

JLinkARM.dll V5.10c (DLL compiled Dec  4 2015 17:25:20)

 

 

 

-----GDB Server start settings-----

 

GDBInit file:                  none

 

GDB Server Listening port:     2331

 

SWO raw output listening port: 2332

 

Terminal I/O port:             2333

 

Accept remote connection:      localhost only

 

Generate logfile:              off

 

Verify download:               on

 

Init regs on start:            on

 

Silent mode:                   off

 

Single run mode:               on

 

Target connection timeout:     0 ms

 

------J-Link related settings------

 

J-Link Host interface:         USB

 

J-Link script:                 none

 

J-Link settings file:          none

 

------Target related settings------

 

Target device:                 MK20DN512XXX10

 

Target interface:              JTAG

 

Target interface speed:        500kHz

 

Target endian:                 little

 

 

 

Connecting to J-Link...

 

J-Link is connected.

 

Firmware: J-Link Ultra Rev.1 compiled Dec  3 2013 14:27:53

 

Hardware: V1.00

 

S/N: 501200180

 

Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB

 

Checking target voltage...

 

Target voltage: 1.79 V

 

Listening on TCP/IP port 2331

 

Connecting to target...ERROR: Bad JTAG communication: Write to IR: Expected 0x1, got 0x5 (TAP Command : 10) @ Off 0xF.

 

 

 

ERROR: Could not connect to target.

 

Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...

 

Shutting down...

 

 

I tried adding the option -jtagconf 0,0 since the kinetis device is the closer to the TDO pin on my board, but I've got the same error

 

Please advise,

Best regards,

Zohar

Labels (1)
0 Kudos
Reply
1 Reply

1,381 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

Check the power supply of the target board. The target voltage 1.79V (see your log) is very low. It can cause the problem.

Best Regards,

Marek Neuzil

0 Kudos
Reply