File locations used by KDS 3.01

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

File locations used by KDS 3.01

1,261 次查看
kevinangus
Contributor III

While trouble shooting a hang issue I started trying to locate where KDS wrote files to:

1. /users/person/ This has a .p2 directory with >800Mb of files

2. /EclipsePath/eclipse/all sorts of files 1.4Gb

3. /ProgramData/Processor Expert/ more files 410Mb

4. /user/person/Appdata/local/Temp more files

5. /user/person/workspace 37Mb 1 project

6. /freescale KSDK 3.27Gb

7. configuration files? When I add this to start eclipse D:\mcu64\eclipse\eclipse.exe -configuration D:\mcu64\configuration in that directory there was files. Without the command line switch I don't know where the files end up.

 

Is there a tool to remove KDS from a computer besides FDISK?

Is there a list where KDS retains files?

标签 (1)
0 项奖励
回复
1 回复

1,148 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Kevin,

assume you are using Linux.What distribution are you using? How did you installed KDS?

Please note that the only supported distributions are Red Hat® Enterprise Linux (RHEL), CentOS 6.4 and Ubuntu 14.04 LTS. All variants of the Kinetis Design Studio software development tools are distributed as 64-bit binaries, which will not work on 32-bit systems.

The proper installation method is decribed here:

http://www.nxp.com/files/microcontrollers/doc/user_guide/KDSUG.pdf


Best regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复