path problem importing default examples for K22

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

path problem importing default examples for K22

3,352件の閲覧回数
jpcordovae
Contributor II

I just bough a FRDM-K22F dev kit, download Kinetics design studio, update and install all I founded, patch the app as I saw here https://community.freescale.com/thread/363937 (I had same problem).

 

Now, I just import one of the examples and I had a bunch of problems with path definitions, the app doesn't found sources and includes, twice worst if I import and copy the project in my workspace.

 

73819_73819.pngworkspace.kds.png

 

73958_73958.pngK22bug.png

 

Watch the path "C:/platform", the SDK and all is installed and running, beacuse I make run and debug some basic programs, and now I need the examples.

 

Pleas someone enlight me, I'm testing this for a new device that I have to develop, but I only have experience with Atmel, TI and PIC microcontrollers and I really want to make run my dev in this plataform.

 

Regards,

 

JPCE

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

3,136件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Juan,

you have incorrectly set paths for the project.

Please, can you check KSDK_PATH in Environment Variables?

ksdk_path.png

Please, take a look at No rule to make target | MCU on Eclipse

Let us know, if it helps you.

Best Regards,

Iva

0 件の賞賛
返信

3,136件の閲覧回数
jpcordovae
Contributor II

Indeed, environment variables are not set :/

Is that a installer bug ?, or I suppose to know that ?

0 件の賞賛
返信

3,136件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

There must be set paths.

Yes, it could be, please try uninstall KSDK and install again.

Best Regards,

Iva

0 件の賞賛
返信

3,136件の閲覧回数
jpcordovae
Contributor II

I did it and doesn't work.

What else can I do.

btw, I just update windows to windows 10 before install kinetics design studio.

JPCE

0 件の賞賛
返信

3,136件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Please, check your steps with Video Link : 3281

Please, do it according to this.

Hope this helps.

Iva

0 件の賞賛
返信

3,136件の閲覧回数
jpcordovae
Contributor II

I uninstall all and install again, and didn't work.

2015-09-14 13_21_43-C_C++ - Kinetis Design Studio - C__Users_JuanPablo_workspace.kds.png

2015-09-14 13_27_26-Install.png

I tried tu put by hand the paths and same problems awnyway.

Now I'm trying to update the paths one by one, long boring task... and I have this problem:

2015-09-15 10_20_56-C_C++ - i2c_rtos_freertos_frdmk22f_board_board.c - Kinetis Design Studio - C__Us.png

2015-09-15 10_33_44-Tienda.png

2015-09-15 10_34_22-C_C++ - i2c_rtos_freertos_frdmk22f_board_hardware_init.c - Kinetis Design Studio.png

complain about definitions/declarations that should be able to handle, and yes, I clean project, refresh, recompile, etc...

JP

0 件の賞賛
返信

3,136件の閲覧回数
ivadorazinova
NXP Employee
NXP Employee

Hi Juan,

Please, can you attach your project? It could be incorrect setting for the toolchain in your project.

Best Regards,

Iva

0 件の賞賛
返信