path problem importing default examples for K22

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

path problem importing default examples for K22

3,453 Views
jpcordovae
Contributor II

I just bough a FRDM-K22F dev kit, download Kinetics design studio, update and install all I founded, patch the app as I saw here https://community.freescale.com/thread/363937 (I had same problem).

 

Now, I just import one of the examples and I had a bunch of problems with path definitions, the app doesn't found sources and includes, twice worst if I import and copy the project in my workspace.

 

73819_73819.pngworkspace.kds.png

 

73958_73958.pngK22bug.png

 

Watch the path "C:/platform", the SDK and all is installed and running, beacuse I make run and debug some basic programs, and now I need the examples.

 

Pleas someone enlight me, I'm testing this for a new device that I have to develop, but I only have experience with Atmel, TI and PIC microcontrollers and I really want to make run my dev in this plataform.

 

Regards,

 

JPCE

Labels (1)
0 Kudos
Reply
7 Replies

3,237 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Juan,

you have incorrectly set paths for the project.

Please, can you check KSDK_PATH in Environment Variables?

ksdk_path.png

Please, take a look at No rule to make target | MCU on Eclipse

Let us know, if it helps you.

Best Regards,

Iva

0 Kudos
Reply

3,237 Views
jpcordovae
Contributor II

Indeed, environment variables are not set :/

Is that a installer bug ?, or I suppose to know that ?

0 Kudos
Reply

3,237 Views
ivadorazinova
NXP Employee
NXP Employee

There must be set paths.

Yes, it could be, please try uninstall KSDK and install again.

Best Regards,

Iva

0 Kudos
Reply

3,237 Views
jpcordovae
Contributor II

I did it and doesn't work.

What else can I do.

btw, I just update windows to windows 10 before install kinetics design studio.

JPCE

0 Kudos
Reply

3,237 Views
ivadorazinova
NXP Employee
NXP Employee

Please, check your steps with Video Link : 3281

Please, do it according to this.

Hope this helps.

Iva

0 Kudos
Reply

3,237 Views
jpcordovae
Contributor II

I uninstall all and install again, and didn't work.

2015-09-14 13_21_43-C_C++ - Kinetis Design Studio - C__Users_JuanPablo_workspace.kds.png

2015-09-14 13_27_26-Install.png

I tried tu put by hand the paths and same problems awnyway.

Now I'm trying to update the paths one by one, long boring task... and I have this problem:

2015-09-15 10_20_56-C_C++ - i2c_rtos_freertos_frdmk22f_board_board.c - Kinetis Design Studio - C__Us.png

2015-09-15 10_33_44-Tienda.png

2015-09-15 10_34_22-C_C++ - i2c_rtos_freertos_frdmk22f_board_hardware_init.c - Kinetis Design Studio.png

complain about definitions/declarations that should be able to handle, and yes, I clean project, refresh, recompile, etc...

JP

0 Kudos
Reply

3,237 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Juan,

Please, can you attach your project? It could be incorrect setting for the toolchain in your project.

Best Regards,

Iva

0 Kudos
Reply