missing debug file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,503件の閲覧回数
randalford
Contributor II

I am trying to create my first project in Kinetis Design Studio will little success. Documentation I have found says to add libraries and path to Settings.Cross Arm C++ Linker.Libraries. It says to add a path to "C:\Freescale\KSDK_1.3.0\lib\ksdk_platform_lib\kds\K22F51212\debug", but this file does not exist. Is there a way to build this file?

 

When do not have this added to the project settings, I get an error: "undefined reference to `GPIO_DRV_WritePinOutput" caused by LED1_EN function. Are these problems somehow related?

 

This is the second Workspace I have tried to create. Can my Workspace be repaired or should I create a new one? I have tried following instructions carefully in setting up a Workspace and am becoming quite frustrated that I cannot get it to work. Please help.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,435件の閲覧回数
randalford
Contributor II
0 件の賞賛
返信
1 返信
1,436件の閲覧回数
randalford
Contributor II

Resolved

0 件の賞賛
返信