kinetics Development Studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kinetics Development Studio

2,476 Views
lijofrancis
Contributor III

Dear Sir,

  i am using KDS with K40 microcontroller (Kwikstik board).why i cant change Generated code(cpu.c ,vector.c...etc)Its automatically generated at startup.if i change ,then after sometime i close the KDS.if i open the project then its automatically generate orignal file.and its overwrite my code .Then my changing function washed away.please tell me how to solve the problem

Another question is by using Kinetic development studio i cant RUN the code,I cant Flash the code.But i can debug and the code is working

is there is any settings or is there any problem. I am using onboard segger jlink (K40 tower board)

Labels (1)
0 Kudos
Reply
5 Replies

2,134 Views
BlackNight
NXP Employee
NXP Employee

Hello,

you have multiple ways/options to disable code generation, see Disable my Code Generation | MCU on Eclipse

Erich

2,134 Views
lijofrancis
Contributor III

hello

i have one more question regarding programmer.i can debug the code but i cant load the code into flash and i cant Run the code .nothing happens error says that GDB closed.i am using KDS with on board segger jlink 

0 Kudos
Reply

2,134 Views
BlackNight
NXP Employee
NXP Employee

Hello,

try clearing all breakpoints/watchpoints, maybe it is this gdb problem described here:

http://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-existi...

Erich

0 Kudos
Reply

2,134 Views
lijofrancis
Contributor III

hello,

There is no breakpoints

when i flash there is on console view

SEGGER J-Link GDB Server V4.92 - Terminal output channel

SEGGER J-Link GDB Server V4.92 Command Line Version

JLinkARM.dll V4.92 (DLL compiled Sep 30 2014 09:33:42)

-----GDB Server start settings-----

GDBInit file:                  none

GDB Server Listening port:     2331

SWO raw output listening port: 2332

Terminal I/O port:             2333

Accept remote connection:      localhost only

Generate logfile:              off

Verify download:               on

Init regs on start:            on

Silent mode:                   off

Single run mode:               on

Target connection timeout:     5 sec.

------J-Link related settings------

J-Link Host interface:         USB

J-Link script:                 none

J-Link settings file:          none

------Target related settings------

Target device:                 MK40DX256xxx10

Target interface:              SWD

Target interface speed:        1000kHz

Target endian:                 little

Connecting to J-Link...

J-Link is connected.

Firmware: J-Link Lite-FSL V1 compiled Jun 25 2012 16:40:07

Hardware: V1.00

S/N: 430110131

Checking target voltage...

Target voltage: 3.15 V

Listening on TCP/IP port 2331

Connecting to target...Connected to target

Waiting for GDB connection...Connected to 127.0.0.1

Reading all registers

Read 4 bytes @ address 0x00000000 (Data = 0x20000000)

Target interface speed set to 1000 kHz

Resetting target

Halting target CPU...

...Target halted (PC = 0x00000A40)

R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000

R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000

R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000

R12= 00000000, R13= 20000000, MSP= 20000000, PSP= 00000000

R14(LR) = FFFFFFFF, R15(PC) = 00000A40

XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000

CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00

Reading all registers

Select auto target interface speed (2000 kHz)

Flash breakpoints enabled

Semi-hosting enabled (VectorAddr = 0x08)

Semihosting I/O set to TELNET Client

Read 4 bytes @ address 0x00000A40 (Data = 0xB082B580)

Downloading 480 bytes @ address 0x00000000 - Verified OK

Downloading 16 bytes @ address 0x00000400 - Verified OK

Downloading 6300 bytes @ address 0x00000410 - Verified OK

Downloading 4 bytes @ address 0x00001CAC - Verified OK

Downloading 4 bytes @ address 0x00001CB0 - Verified OK

Downloading 668 bytes @ address 0x00001CB4 - Verified OK

Downloading 36 bytes @ address 0x00001F50 - Verified OK

Read 4 bytes @ address 0x00000A40 (Data = 0xB082B580)

0 Kudos
Reply

2,134 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Lijo Francis:

Just checking, did you solve this problem with your KwikStik?

If not it may be due to the MCU selection from the New Project Wizard or the J-Link Debugger settings. Check the next discussion for pointers:

Re: IDE for KwikStik

Regards!

Jorge Gonzalez

0 Kudos
Reply