getting An internal error occurred during: "Launching hello_world_frdmk64f debug cmsisdap". ilg.gnuarmeclipse.debug.gdbjtag.dsf.GnuArmServicesFactory.<init>(Ljava/lang/String;Ljava/lang/String;)V error when try to debug hello world demo

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

getting An internal error occurred during: "Launching hello_world_frdmk64f debug cmsisdap". ilg.gnuarmeclipse.debug.gdbjtag.dsf.GnuArmServicesFactory.<init>(Ljava/lang/String;Ljava/lang/String;)V error when try to debug hello world demo

2,966 次查看
saficifci
Contributor I

Any Solution?

91311_91311.pngpastedImage_0.png

标签 (1)
0 项奖励
回复
7 回复数

2,336 次查看
saficifci
Contributor I

Thanks,Erich I will try it

0 项奖励
回复

2,336 次查看
BlackNight
NXP Employee
NXP Employee

Ok, so then I think the problem it is really because you have updated that plugin. Using P&E is not affected by that updated, but Segger J-Link for sure is, and it seems that it affects as well OpenOCD.

In case you need to use OpenOCD or J-Link, then you have to apply the patch from Unable to Debug after KDS Update .

Erich

2,336 次查看
anthony_huereca
NXP Employee
NXP Employee

I was having the same issue, and updating the Eclipse plugin as described in that thread fixed this for me.

2,336 次查看
antbe
Contributor I

+1

This updating solves the problem for OpenOCD too. Thanks!

0 项奖励
回复

2,336 次查看
saficifci
Contributor I

Hi Erich ,

The plugins are as follow , Anyway I have solved my problem by using PE Debugging , now it works

pastedImage_0.png

0 项奖励
回复

2,336 次查看
BlackNight
NXP Employee
NXP Employee

Could it be that you have updated the GNU ARM Eclipse plugins?

This is what I have and is working for me:

pastedImage_0.png

Note that there had been a GNU ARM Eclipse update which breaks at least the segger J-link debugging (I had not observed that it breaks OpenOCD).

Have a look at Unable to Debug after KDS Update  which as well includes the patch/workaround.

Can you apply that patch and check if this helps?

I hope this helps,

Erich

0 项奖励
回复

2,336 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

1. please make sure you didn't import the projects with breakpoints.

2. regarding you use FRDM-K64F board, I suggest you check this article for several method to connect to FRMD-K64F board.

Summary of FRDM-K64F open source debug interface

3. if you want to use CMSIS-DAP debug interface anyway,

You can download CMSIS-DAP deliverables from ARM via the link below (requires login).

https://silver.arm.com/browse/CMSISDAP

Can this help you?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复