about KSDK 1.0.0   mqx lib  KDS build support.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about KSDK 1.0.0   mqx lib  KDS build support.

ソリューションへジャンプ
3,164件の閲覧回数
haidong_zheng
NXP Employee
NXP Employee

KSDK lib/ksdk_mqx_lib/kds/K22F51212/ directory only has one fle : makedir.bat, seem this version dose not include KDS build support.

While for GCC mqx lib Makefile,  there is a error in KSDK

lib/ksdk_mqx_lib/gcc/K22F51212/Makefile

LIB_NAME = ksdk_platform_lib   it should be ksdk_mqx_lib.

 

 

There is one interesting thing:

KSDK has GCC  mqx lib support, while MQX_KSDK  beta release dose not support GCC build.

 




ラベル(1)
0 件の賞賛
返信
1 解決策
2,679件の閲覧回数
haidong_zheng
NXP Employee
NXP Employee

KSDK lib/ksdk_mqx_lib/kds/K22F51212/ directory only has one fle : makedir.bat, seem this version dose not include KDS build support.

This directory has another "dot" start files, those are KDS project files, so this directory can be imported as KDS root project directory.


元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
2,679件の閲覧回数
xinyu_chen
NXP Employee
NXP Employee

Hi Haidong

I checked the formal 1.0.0 GA release, I have the .cproject and .project files under lib/ksdk_mqx_lib/kds/K22F51212/

pastedImage_0.png

For the lib\ksdk_mqx_lib\gcc\K22F51212\Makefile file, actually, we only support MQX lib build in KDS, not in the GCC command line.

So this file is not usable.

0 件の賞賛
返信
2,680件の閲覧回数
haidong_zheng
NXP Employee
NXP Employee

KSDK lib/ksdk_mqx_lib/kds/K22F51212/ directory only has one fle : makedir.bat, seem this version dose not include KDS build support.

This directory has another "dot" start files, those are KDS project files, so this directory can be imported as KDS root project directory.


0 件の賞賛
返信
2,679件の閲覧回数
xinyu_chen
NXP Employee
NXP Employee

Hi Haidong

You mean the KDS 1.1 with KSDK 1.0 GA release? There's no KSDK_1.1.0 release yet.

0 件の賞賛
返信
2,679件の閲覧回数
haidong_zheng
NXP Employee
NXP Employee
0 件の賞賛
返信
2,675件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi!

My KSDK installation shows the project of the library you are missing (you can see attached image). I think you need to go to menu Help > Install New Software > select Freescale KDS Update Site and install all the updates.

Regards,

Carlos

0 件の賞賛
返信
2,675件の閲覧回数
haidong_zheng
NXP Employee
NXP Employee

Sorry, KSDK is 1.0.0

0 件の賞賛
返信
2,675件の閲覧回数
YixingKong
Senior Contributor IV

Xinyu Chen, could you please help in answering the build issue?

Thanks,

Yixing

0 件の賞賛
返信