about KSDK 1.0.0   mqx lib  KDS build support.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about KSDK 1.0.0   mqx lib  KDS build support.

Jump to solution
3,032 Views
haidong_zheng
NXP Employee
NXP Employee

KSDK lib/ksdk_mqx_lib/kds/K22F51212/ directory only has one fle : makedir.bat, seem this version dose not include KDS build support.

While for GCC mqx lib Makefile,  there is a error in KSDK

lib/ksdk_mqx_lib/gcc/K22F51212/Makefile

LIB_NAME = ksdk_platform_lib   it should be ksdk_mqx_lib.

 

 

There is one interesting thing:

KSDK has GCC  mqx lib support, while MQX_KSDK  beta release dose not support GCC build.

 




Labels (1)
0 Kudos
Reply
1 Solution
2,547 Views
haidong_zheng
NXP Employee
NXP Employee

KSDK lib/ksdk_mqx_lib/kds/K22F51212/ directory only has one fle : makedir.bat, seem this version dose not include KDS build support.

This directory has another "dot" start files, those are KDS project files, so this directory can be imported as KDS root project directory.


View solution in original post

0 Kudos
Reply
7 Replies
2,547 Views
xinyu_chen
NXP Employee
NXP Employee

Hi Haidong

I checked the formal 1.0.0 GA release, I have the .cproject and .project files under lib/ksdk_mqx_lib/kds/K22F51212/

pastedImage_0.png

For the lib\ksdk_mqx_lib\gcc\K22F51212\Makefile file, actually, we only support MQX lib build in KDS, not in the GCC command line.

So this file is not usable.

0 Kudos
Reply
2,548 Views
haidong_zheng
NXP Employee
NXP Employee

KSDK lib/ksdk_mqx_lib/kds/K22F51212/ directory only has one fle : makedir.bat, seem this version dose not include KDS build support.

This directory has another "dot" start files, those are KDS project files, so this directory can be imported as KDS root project directory.


0 Kudos
Reply
2,547 Views
xinyu_chen
NXP Employee
NXP Employee

Hi Haidong

You mean the KDS 1.1 with KSDK 1.0 GA release? There's no KSDK_1.1.0 release yet.

0 Kudos
Reply
2,547 Views
haidong_zheng
NXP Employee
NXP Employee
0 Kudos
Reply
2,544 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi!

My KSDK installation shows the project of the library you are missing (you can see attached image). I think you need to go to menu Help > Install New Software > select Freescale KDS Update Site and install all the updates.

Regards,

Carlos

0 Kudos
Reply
2,544 Views
haidong_zheng
NXP Employee
NXP Employee

Sorry, KSDK is 1.0.0

0 Kudos
Reply
2,544 Views
YixingKong
Senior Contributor IV

Xinyu Chen, could you please help in answering the build issue?

Thanks,

Yixing

0 Kudos
Reply