Why there is no 64-bit DEB package for Kinetis Design Studio?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why there is no 64-bit DEB package for Kinetis Design Studio?

跳至解决方案
1,195 次查看
adrianomitre
Contributor II

Why Freescale does not offer a 64-bit DEB package for Kinetis Design Studio? It is very inconvenient having to keep both a 32-bit and 64-bit Java Development Kits, not to mention the probable performance hit from not using x86-64-specific instructions.

 

SEGGER offers DEB Installer 64-bit version of their J-Link drivers and I think Freescale should do the same for KDS, specially given that virtually all desktops now run 64-bit processors and probably most Debian based GNU/Linux installs are also 64-bit.

标签 (1)
标记 (5)
1 解答
1,077 次查看
BlackNight
NXP Employee
NXP Employee

The version V2.0.0 coming out to the end of this year will be 64bit. We had an initernal depency on 32bit binaries, and it was not possible to change that to 64bit in the time frame for the V1.x release. I agree that the 32bit binaries are not ideal, but in my view better than everyone had to wait for the 64bit version at the end of the year. I hope that makes sense.

Erich

在原帖中查看解决方案

1 回复
1,078 次查看
BlackNight
NXP Employee
NXP Employee

The version V2.0.0 coming out to the end of this year will be 64bit. We had an initernal depency on 32bit binaries, and it was not possible to change that to 64bit in the time frame for the V1.x release. I agree that the 32bit binaries are not ideal, but in my view better than everyone had to wait for the 64bit version at the end of the year. I hope that makes sense.

Erich