Why there is no 64-bit DEB package for Kinetis Design Studio?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why there is no 64-bit DEB package for Kinetis Design Studio?

ソリューションへジャンプ
1,252件の閲覧回数
adrianomitre
Contributor II

Why Freescale does not offer a 64-bit DEB package for Kinetis Design Studio? It is very inconvenient having to keep both a 32-bit and 64-bit Java Development Kits, not to mention the probable performance hit from not using x86-64-specific instructions.

 

SEGGER offers DEB Installer 64-bit version of their J-Link drivers and I think Freescale should do the same for KDS, specially given that virtually all desktops now run 64-bit processors and probably most Debian based GNU/Linux installs are also 64-bit.

ラベル(1)
タグ(5)
1 解決策
1,134件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The version V2.0.0 coming out to the end of this year will be 64bit. We had an initernal depency on 32bit binaries, and it was not possible to change that to 64bit in the time frame for the V1.x release. I agree that the 32bit binaries are not ideal, but in my view better than everyone had to wait for the 64bit version at the end of the year. I hope that makes sense.

Erich

元の投稿で解決策を見る

1 返信
1,135件の閲覧回数
BlackNight
NXP Employee
NXP Employee

The version V2.0.0 coming out to the end of this year will be 64bit. We had an initernal depency on 32bit binaries, and it was not possible to change that to 64bit in the time frame for the V1.x release. I agree that the 32bit binaries are not ideal, but in my view better than everyone had to wait for the 64bit version at the end of the year. I hope that makes sense.

Erich