Where can i find documentation for the shell for sdk 1.3???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can i find documentation for the shell for sdk 1.3???

1,147 Views
jasonscott
Contributor IV


Hi all,

 

I have been struggling to find decent documentation on how to integrate a shell application with the processor expert.

 

I have noticed numerous tutorials using the 1.2 sdk.(Currently downloading).

 

I had assumed that they would all build on one another, but i have had no luck.

 

Most of the example code is set up for certain boards and not individual processors(which i am okay with, i can link the libraries myself). What i cant understand is the integration of the code warrior c examples.

 

I figured the IDE would make things simple....

 

Am i just making things harder than they need to be?

 

Any pointers would be appreciated!

 

BTW.... I am using the KDS 3.2 and currently working with SDK 1.3.

 

-Jason

Labels (1)
0 Kudos
Reply
2 Replies

918 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I would suggest you refer this discussion:

Where is the documentation or examples for the Shell included in the KSDK 1.3 created by the KSDK Bu...

Can it help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

918 Views
jasonscott
Contributor IV

Hi Jennie,

It was enlightening, but still does not help me with my current problem.

I am expected to include the "shell" from the old MQX project, but I can not find a way to make it work with the processor expert.

Thanks for your time,

Jason

0 Kudos
Reply