Using USB module code generated by KDS processor expert cannot enum my device,why?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using USB module code generated by KDS processor expert cannot enum my device,why?

Jump to solution
2,365 Views
haibodeng
Contributor I

Hi:

 

We just have a board with the processor type MK64FN1M0VLQ12. And we use the KDS processor expert to generate the module low level drivers.

But it has a problem as follows.

When we want to test the USB interface,we call the functions supported by the USB1.c just like the help document says,but I found it can not enum

my device.

I can receive the first setup packet from the host .It request a device descriptor,and I send my descriptor to the host. Next to it ,I found the host reset

my device and request a device descriptor again. I send my descriptor again,and the host reset my device.

The host reset my device 4 times and the suspend it.Why?

 

I think the host will send a set address request following the device descriport request,but I never receive it.

 

Can anyone help me?Thanks very much.

 

Here is my usb.c and debug information:

37086_37086.pngpastedImage_54.png

/*

* usb.c

*

*  Created on: 2015年4月15日

*  Author: Denghaibo

*/

#include "Cpu.h"

#include "Events.h"

#include "Pins1.h"

#include "USB1.h"

 

 

/* Including shared modules, which are used for whole project */

#include "PE_Types.h"

#include "PE_Error.h"

#include "PE_Const.h"

#include "IO_Map.h"

#include "PDD_Includes.h"

#include "Init_Config.h"

#include "stdio.h"

#include "common.h"

 

TMyDevData MyDevData;

bool CallbackCalled = FALSE;

 

 

void Callback(LDD_TDeviceData *pDevData, LDD_USB_Device_TTD* pTD)

{

  word Sn;

  printStr("DataTDPtr done!\r\n");

  pTD->CallbackFnPtr = 0;

}

void Callback1(LDD_TDeviceData *pDevData, LDD_USB_Device_TTD* pTD)

{

  word Sn;

  printStr("HskTDPtr done!\r\n");

   pTD->CallbackFnPtr = 0;

}

 

extern LDD_USB_TDevDescriptor MyUSBDevDescriptor;

extern uint8_t USB_Config_Descriptor[9+9+7+7];

extern LDD_USB_TEpDescriptor USB_Ep1OutDescriptor;

extern LDD_USB_TEpDescriptor USB_Ep1InDescriptor;

extern uint8_t Language[4];

extern unsigned char ManufacturerStr[22];

extern unsigned char ProductStr[16];

extern unsigned char SerialNumberStr[26];

 

LDD_TError USER_USB1_DevInitEndpoint(LDD_TUserData *UserDataPtr)

{

  LDD_TError error = ERR_OK;

  TMyDevData *tMyDevData = (TMyDevData *)UserDataPtr;

  error = USB1_DeviceInitEndpoint((LDD_TDeviceData *)tMyDevData->USB1_LDDDevDataPtr, (LDD_USB_TEpDescriptor *)&MyUSBDevDescriptor, 0x00);

  return error;

}

/*

** ==================================================================

**     Method      :  USER_USB_init (void)

*/

/*!

**     @brief

**         Call the driver function USB1_Init(),then enable the pull-up

**         resister, wait for the host to config the USBFS.

**     @param

**         UserDataPtr     - NULL

**     @return

**                         - NULL

*/

/* ===================================================================*/

 

LDD_TError USER_USB_init(void)

{

  LDD_TError error = ERR_OK;

   MyDevData.USB1_LDDDevDataPtr = USB1_Init((LDD_TUserData *)&MyDevData);         /* Initialize the device */

      USB0_USBCTRL=0x40;

   error = USB1_Enable(MyDevData.USB1_LDDDevDataPtr);

   return error;

}

/*

* 标准请求

*/

#define USB_DEV_GET_STATUS 0x00

#define USB_DEV_CLR_FEATURE 0x01

#define USB_DEV_SET_FEATURE 0x03

#define USB_DEV_SET_ADDRESS 0x05

#define USB_DEV_GET_DESCRIPTOR 0x06

#define USB_DEV_SET_DESCRIPTOR 0x07

#define USB_DEV_GET_CONFIG   0x08

#define USB_DEV_SET_CONFIG   0x09

#define USB_DEV_GET_INTERFACE   0x0A

#define USB_DEV_SET_INTERFACE   0x0B

#define USB_SYNCH_FRAME   0x0C

 

uint8_t bAsciiBuffer[100];

 

void USER_USB1_OnDeviceSetupPacket(LDD_TUserData *UserDataPtr, uint8_t EpNum)

{

  TMyDevData *MyDevDataPtr = (TMyDevData *)UserDataPtr;

  LDD_TDeviceData *USB_LDDDevDataPtr = MyDevDataPtr->USB1_LDDDevDataPtr;

  LDD_USB_TSDP                    *pSDP = &MyDevDataPtr->SDP;

 

 

  LDD_USB_Device_TTD              *DataTDPtr = &MyDevDataPtr->DataTD;//

  LDD_USB_Device_TTD              *HskTDPtr = &MyDevDataPtr->HskTD;

  LDD_TError                       res = ERR_OK;

  int                              DestIdx;

  uint8_t* pSetupData;

  uint8_t i;

  uint16_t bBytesSend,error;

 

  USB1_DeviceReadSetupData(USB_LDDDevDataPtr,EpNum,pSDP);

 

  DataTDPtr->Head.EpNum      = 0x00u;

  DataTDPtr->Head.BufferPtr  = NULL;

  DataTDPtr->Head.BufferSize = 0x00u;

  DataTDPtr->Head.Flags      = 0x00;

 

  charChangeToAscii((byte*)pSDP,(byte*)bAsciiBuffer,8);

  AS1_SendBlock((byte*)&bAsciiBuffer[0],26,&bBytesSend);

 

   if ((pSDP->bmRequestType & LDD_USB_REQ_RECP_MASK) == LDD_USB_REQ_RECP_DEVICE) {

      /* Request for Device */

      switch(*((uint8*)&(pSDP->bRequest))) { /* Depend on request type call do: */

 

      case USB_DEV_GET_DESCRIPTOR: //获取描述符

 

      if(((pSDP->wValue >> 8)&0xff) == LDD_USB_DT_DEVICE)

      {

   DataTDPtr->Head.EpNum      = EpNum;

   DataTDPtr->Head.BufferPtr  = (LDD_TData*)&MyUSBDevDescriptor;

   DataTDPtr->Head.BufferSize = MyUSBDevDescriptor.bLength;

   DataTDPtr->Head.Flags      = LDD_USB_DEVICE_TRANSFER_FLAG_EXT_PARAM;

   DataTDPtr->CallbackFnPtr   = Callback;

   DataTDPtr->ParamPtr = 0;

      }

      else if(((pSDP->wValue >> 8)&0xff) == LDD_USB_DT_CONFIGURATION)

      {

   DataTDPtr->Head.EpNum      = EpNum;

   DataTDPtr->Head.BufferPtr  = (LDD_TData*)&USB_Config_Descriptor;

   DataTDPtr->Head.BufferSize = pSDP->wLength;

   DataTDPtr->Head.Flags      = 0;//LDD_USB_DEVICE_TRANSFER_FLAG_EXT_PARAM;

   DataTDPtr->CallbackFnPtr   = Callback;

   DataTDPtr->ParamPtr = 0;

      }

      else if(((pSDP->wValue >> 8)&0xff) == LDD_USB_DT_STRING)

      {

  if((pSDP->wValue&0xff) == 0)

  {

   DataTDPtr->Head.EpNum      = EpNum;

   DataTDPtr->Head.BufferPtr  = (LDD_TData*)&Language;

   DataTDPtr->Head.BufferSize = 0x04;

  }

  else if((pSDP->wValue&0xff) == 1)//索引1

  {

   DataTDPtr->Head.EpNum      = EpNum;

   DataTDPtr->Head.BufferPtr  = (LDD_TData*)&ManufacturerStr;

   DataTDPtr->Head.BufferSize = sizeof(ManufacturerStr);

  }

  else if((pSDP->wValue&0xff) == 2)//索引2

  {

   DataTDPtr->Head.EpNum      = EpNum;

   DataTDPtr->Head.BufferPtr  = (LDD_TData*)&ProductStr;

   DataTDPtr->Head.BufferSize = sizeof(ProductStr);

  }

  else if((pSDP->wValue&0xff) == 3)//索引3

  {

   DataTDPtr->Head.EpNum      = EpNum;

   DataTDPtr->Head.BufferPtr  = (LDD_TData*)&SerialNumberStr;

   DataTDPtr->Head.BufferSize = sizeof(SerialNumberStr);

  }

      }

      break;

        case USB_DEV_SET_ADDRESS:

          /* Note: USB State of the device is changed after successful status stage of transaction */

          /* Send zero-length data packet and set callback for this packet */

      DataTDPtr->Head.EpNum   = EpNum;

          DataTDPtr->Head.BufferSize    = 0x00;

 

 

          USB_PDD_WriteAddressReg(USB0_BASE_PTR, (((LDD_USB_TSetAddressRequest*)pSDP)->DeviceAddress));      /* Set device address to the 0 value */

          break;

        case USB_DEV_SET_CONFIG:

      DataTDPtr->Head.EpNum   = EpNum;

          DataTDPtr->Head.BufferSize    = 0x00;

      break;

        default:

          res = ERR_NOTAVAIL;

        break;

      }

    } else if ((pSDP->bmRequestType & LDD_USB_REQ_RECP_MASK) == LDD_USB_REQ_RECP_INTERFACE) {

      /* Request for Interface */

      DestIdx = (uint8_t)pSDP->wIndex;

  #define MAX_INTERFACE_NUMBER 1

      if (DestIdx > MAX_INTERFACE_NUMBER) {

        res = ERR_FAILED;                /* Interface number too big */

      } else {

 

      }

    } else if ((pSDP->bmRequestType & LDD_USB_REQ_RECP_MASK) == LDD_USB_REQ_RECP_ENDPOINT) {

      /* Request for Endpoint */

      DestIdx = ((uint8_t)pSDP->wIndex << 0x01) & 0xFF;

      if (pSDP->wIndex & 0x80) { /* IN(Tx) EP? */

        DestIdx |= 0x01;

      }

  #define MAX_EP_IDX 1

      if (DestIdx > MAX_EP_IDX) {

        res = ERR_FAILED;                /* Endpoint number too big */

      } else {

 

 

      }

    } else {

      /* Request for Other */

      res = ERR_NOTAVAIL;

    }

 

    if (res == ERR_OK) {

      HskTDPtr->Head.BufferSize = 0x00;

      HskTDPtr->Head.EpNum   = EpNum;

      HskTDPtr->Head.Flags      = LDD_USB_DEVICE_TRANSFER_FLAG_EXT_PARAM;

      HskTDPtr->CallbackFnPtr   = Callback1;

      HskTDPtr->ParamPtr   = 0;

      printStr("Return data:");

 

  charChangeToAscii((byte*) DataTDPtr->Head.BufferPtr,(byte*)bAsciiBuffer,DataTDPtr->Head.BufferSize);

  AS1_SendBlock((byte*)&bAsciiBuffer[0],DataTDPtr->Head.BufferSize * 3 + 2,&bBytesSend);

 

      if (pSDP->wLength == 0x00) {

        /* No data */

        DataTDPtr->Head.BufferSize = 0x00u;                   /* Send Zero-length data packet */

        (void)USB1_DeviceSendData(USB_LDDDevDataPtr, DataTDPtr);

      } else if (pSDP->bmRequestType & LDD_USB_DIR_IN) {

        /* Control read */

        error = USB1_DeviceSendData(USB_LDDDevDataPtr, DataTDPtr);

        error = USB1_DeviceRecvData(USB_LDDDevDataPtr, HskTDPtr);

      } else {

        /* Control write */

        (void)USB1_DeviceRecvData(USB_LDDDevDataPtr, DataTDPtr);

        (void)USB1_DeviceSendData(USB_LDDDevDataPtr, HskTDPtr);

      }

    }

    if (res != ERR_OK) {

      (void)USB1_DeviceStallEndpoint(USB_LDDDevDataPtr, 0x00, 0x00);

      /* Command is not handled or command error*/

    }

}

 

!

Original Attachment has been moved to: MK64-0606.rar

Labels (1)
1 Solution
2,140 Views
jiri_rezler
NXP Employee
NXP Employee

Hello,

I'm checked attached project. I found two significant problems:

1) USB descriptors (Device, Configuration, ...) are placed in Flash memory area.

USB module access to flash memory is through AXBS module. In AXBS module, access between USB module and Flash memory area is disabled (after MCU reset). For configuration USB memory access is possible to use "Init_FMC" component (by "Access protection" property - set to "Read only" value for Master4/USB OTG module):

pastedImage_9.png

2) Problem with MCU BUS priority.

In main() function is code:

pastedImage_18.png

=> In this case is MCU internal BUS "fully" allocated by MCU ARM core. After MCU reset, ARM code BUS has maximal priority = 1 and USB OTG module = 5.

For BUS priority configuration is possible to use "Init_AXBS" component and set properties "ARM core code BUS" = 5,  "USB OTG" module = 1 (e.g.):

pastedImage_19.png

Fixed project is attached.

Best Regards,

Jiri Rezler

View solution in original post

2 Replies
2,141 Views
jiri_rezler
NXP Employee
NXP Employee

Hello,

I'm checked attached project. I found two significant problems:

1) USB descriptors (Device, Configuration, ...) are placed in Flash memory area.

USB module access to flash memory is through AXBS module. In AXBS module, access between USB module and Flash memory area is disabled (after MCU reset). For configuration USB memory access is possible to use "Init_FMC" component (by "Access protection" property - set to "Read only" value for Master4/USB OTG module):

pastedImage_9.png

2) Problem with MCU BUS priority.

In main() function is code:

pastedImage_18.png

=> In this case is MCU internal BUS "fully" allocated by MCU ARM core. After MCU reset, ARM code BUS has maximal priority = 1 and USB OTG module = 5.

For BUS priority configuration is possible to use "Init_AXBS" component and set properties "ARM core code BUS" = 5,  "USB OTG" module = 1 (e.g.):

pastedImage_19.png

Fixed project is attached.

Best Regards,

Jiri Rezler

2,140 Views
haibodeng
Contributor I

Hello:

Thanks very much.Your answer fully solve my problem.

Best Regards,

Haibo Deng

0 Kudos
Reply