Using OSX version of KDS with CMSIS-DAP firmware on FRDM-KLxx boards.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using OSX version of KDS with CMSIS-DAP firmware on FRDM-KLxx boards.

1,131 Views
fmiku
Contributor III

Hi folks,

 

I figured out how to get a working configuration with FRDM-KL25Z board.

 

I'm new on this platform and I want to use OSX or Linux for developing.

 

I do the following steps to get working:

 

           By default the FRDM-KL2x boards are not supported, for support install the KDSK 1.3 (KSDK 2.0 is released but not tested yet)

          After installing run KDS again, go Help->Install New software->Add->Arhive

          and browse to the file "KSDK_INSTALL_DIRECTORY"/tools/eclipse_update/KSDK_1.3.0_Eclipse_Update.zip

         

     List of supported boards after integrating KSDK-1.3 into the KDS.

          120061_120061.pngboards.png

 

          A stable version is available if you have any problem with the -dev version. gnuarmeclipse-openocd-osx-0.9.0-201505191004.pkg

 

  • Add eclipse support for OpenOCD Debug.

          Download the file and install the plugin (Help->Install New software->Add->Arhive) ilg.gnuarmeclipse.repository-2.11.1-201512141335.zip

          Seclect the OpenOCD Debug and others if you want.

 

          120063_120063.pngopenocd.png

 

          after install you need to set the correct path for the openocd binaries.

          Go to the Kninetis Design Studio -> Preferences menu and set the path.

          120064_120064.pngopenocd-bin.png

          steps for install: https://developer.mbed.org/handbook/Firmware-FRDM-KL25Z

 

    

  • Now Ready to start
    • Start a new project as NEW->Kinetis SDK 1.x Project
    • Choose a name
    • Choose a Board or processor
    • Select the Kinetis SDK with ABSOLUTE PATH and add PE support
      • (of course you need to set your own installation path)
      • 120308_120308.pngKépernyőfotó 2015-12-25 - 19.31.14.png
      • at the next step choose the GNU C compiller
      • After Finish make a new debug configuration in your project's settings as follows
        • 120309_120309.pngdebug cfg.png

 

              

And... Finally get working

120062_120062.pngFinal.png

Labels (1)
0 Replies