KDS for Mac - Freeze on launch, can't select workspace

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS for Mac - Freeze on launch, can't select workspace

1,194 Views
jacobjennings
Contributor III

I would love to work on my Mac laptop without needing a VM or Windows dual-boot, but when I install and launch KDS 3.0.0 on OS X 10.11.1 (15B42), I see the workspace selection popup, but the UI does not response to mouse or keyboard. Anyone else using KDS for Mac? Is there a way to manually specify the workspace in a configuration file and skip the initial popup?

 

Thanks,

Jake

 

Edit: I managed to figure out how to specify my workspace and skip the initial popup. It seems to load my workspace just fine, but it still does not respond to any mouse or keyboard input at all.

 

Edit, solution for posterity: Release notes for KDS 3.1.0 under known issues has a fix for this issue (KDS-343 in the document)

Labels (1)
Tags (2)
1 Reply

812 Views
BlackNight
NXP Employee
NXP Employee

The issue is described here as well: KDS on OS X El Capitan (Beta)

Erich