USB STACK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB STACK

2,235 Views
kooroshhajiani
Contributor III

Hi,

How do I download and  install USB CDC Class component  from USB stack 4.03 for KDS ProcessorExpert?

I NEED A CDC DEVICE FOR K20 BOARDS.

 

Where is USB stack 4.03?

 

 

Thanks,

Koorosh Hajiani

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,501 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Koorosh Hajiani,

we can download USB Stack v4.0.3 from here:

USB Stack|NXP

however, usb stack v4.0.3 is a very old version, officially it was tested under Codewarrior 10,IAR, Keil only. see below developement tools requirement:

pastedImage_7.png

fortunately, Erich has article regarding use USB stack v4.1.1 processor expert with KDS. you could refer

USB CDC with the FRDM-K64F, finally! | MCU on Eclipse

I suggest you use KDS+KSDK processor expert to implement USB. refer these articles:

Creating a New USB project with KSDK and Processor Expert support in KDS

How to implement a USB Device MSD demo based on KSDK PEx components and KDS 3.0

Can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------