Testing without hardware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Testing without hardware

2,021件の閲覧回数
piotrek
Contributor III

I would like to develop and test (including execution time/CPU cycles) some algorithms without a hardware.

Is this possible?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,785件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello piotrek:

Kinetis Design Studio does not support chip simulation, so it is not possible.

From your posts I think you are using FRDM-K64, so the next post by peer developer Mark Butcher in the community about uTasker might be interesting for you:

New Freedom FRDM-K64F board


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,785件の閲覧回数
piotrek
Contributor III

Hi Jorge,

Thanks for a very interesting information on uTasker but I don't think I can use it to optimize my DSP loops. For now it seems that a couple of I/O pins and an oscilloscope are my best friends.

EDIT:

K64 seems to implement DWT_CYCCNT Cycle Count Register. Is this register accessible through the KDS IDE?

Regards,

Piotr

0 件の賞賛
返信