TWR-K70 OSC0 Setting in KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TWR-K70 OSC0 Setting in KDS

跳至解决方案
818 次查看
waqasbutt
Contributor II

On TWR-K70 OSC0 is 50MHz. I can't set it in KDS. Any ideas?

 

174849_174849.pngPicture 2017-01-20 09_38_46.png

标签 (1)
0 项奖励
回复
1 解答
706 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Waqas Butt,

You select clock source as "crystal", however the maximal crystal value is 32Mhz.

you need select clock source as "External reference clock" which allows to set 50MHz clock frequency .

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
707 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Waqas Butt,

You select clock source as "crystal", however the maximal crystal value is 32Mhz.

you need select clock source as "External reference clock" which allows to set 50MHz clock frequency .

pastedImage_1.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复