TWR-K65F180M Debug Config Setup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K65F180M Debug Config Setup

ソリューションへジャンプ
2,331件の閲覧回数
henninjw
Contributor II

I have just started using the TWR-K65F180M and am running through setting up the debug configurations as laid out in the getting started with KSDK videos.  The issue I am having is when setting up the PEMicro Interface Port I have no port options(see picture below). Examples I have seen "USB1 - OpenSDA" example is available and selected. How do I achieve this?

135623_135623.pngpastedImage_3.png

ラベル(1)
1 解決策
2,033件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Jake,

Did you update the TWR-K65F180M debugging firmware to support Pemicro?

If not the ZIP is attached.  Unplug the USB debug cable, hold reset button down, plug-in USB debug cable, and system should enumerate as a MSD.

Then drag-n-drop the *.bin file to the BOOTLOADER disk.  After a few seconds new firmware should be loaded.  Unplug and re-plug and you should have the Pemico OpenSDA interface enumerated.

Then back in debugger you should see it.

Regards,

David

PS ignore the name of the ZIP and file...it really does work with TWR-K65F180M.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,034件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Jake,

Did you update the TWR-K65F180M debugging firmware to support Pemicro?

If not the ZIP is attached.  Unplug the USB debug cable, hold reset button down, plug-in USB debug cable, and system should enumerate as a MSD.

Then drag-n-drop the *.bin file to the BOOTLOADER disk.  After a few seconds new firmware should be loaded.  Unplug and re-plug and you should have the Pemico OpenSDA interface enumerated.

Then back in debugger you should see it.

Regards,

David

PS ignore the name of the ZIP and file...it really does work with TWR-K65F180M.

0 件の賞賛
返信
2,033件の閲覧回数
henninjw
Contributor II

Thank you David

0 件の賞賛
返信