Seggar J-Trace Cortex-M

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Seggar J-Trace Cortex-M

ソリューションへジャンプ
1,818件の閲覧回数
calvinday
Contributor III

Does the KDS support the Seggar J-Trace Cortex-M?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,549件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

"CodeWarrior comes with a built-in trace viewer and support for hardware trace, while something like this is not present in KDS."

So, KDS doesn't support J-trace trace feature but CodeWarrior10.6 does.

to summary, All the J-trace trace related feature is not supported by KDS, but you can use the J-Trace as normal debug interface (without tracing) with KDS.

does this answer your question?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,550件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

"CodeWarrior comes with a built-in trace viewer and support for hardware trace, while something like this is not present in KDS."

So, KDS doesn't support J-trace trace feature but CodeWarrior10.6 does.

to summary, All the J-trace trace related feature is not supported by KDS, but you can use the J-Trace as normal debug interface (without tracing) with KDS.

does this answer your question?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信