SPI PEx component not supported by KL27Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI PEx component not supported by KL27Z

2,521件の閲覧回数
joe_dimaggio
Contributor II


Hi,

 

I'm trying to create a datalogger application using a custom layout based on the Kinetis MKL27Z256VFT4 and the FAT file system PEx component.

After selecting SD card and the other components, the SPI PEx component isn't supported with this processor, where is the problem ???

 

My setup:

KDS 3.2.0

KSDK 1.3.0

Processor Expert Components (03.04.2016)

Windows 7 (32 bit)

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,376件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Gianluca,

Could you please take a screenshot about why do you think it doesn't support the SPI.

On my side,  i create one project, then can add the SPI component :

pastedImage_0.png

Hope it helps

Alice

0 件の賞賛
返信

2,376件の閲覧回数
joe_dimaggio
Contributor II

Hello Alice,

sorry for the late reply, I worked on another project last days.

As you can see several processor experts components don't work with this processor: SPI, Timer, SD-Card...

The main component I need is FAT_FileSystem (with SD_Card), but this is not included in the KSDK 1.3.0.

KL27_PEx_error_1.jpg

0 件の賞賛
返信

2,376件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Gianluca,

If your project is KSDK project,  you can not use the PE component without KSDK,

only can use the KSDK PE component :

pastedImage_0.png

there is the SD card component :

pastedImage_1.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,376件の閲覧回数
joe_dimaggio
Contributor II

not really, because I need a FAT component as I'm a newbie.

But Erich Styger wrote an interesting article about how to merge KSDK 2.0 and processor expert:

https://mcuoneclipse.com/2016/05/15/mother-of-components-processor-expert-with-nxp-kinetis-sdk-v2-0-...

thanks anyway!

0 件の賞賛
返信