Programming MKL24Z32VFT4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming MKL24Z32VFT4

2,854 Views
hb0038
Contributor II

Hi, 

I developed a custom development board using NXP MKL24Z32VFT4 32bit 48QFN microcontroller. For the programming my board I took out SWD pins. What are the possible programmers/debuggers can I use to programme my custom board? 

If I buy FRDM-KL26Z development platform can I use it as a programmer?

Thanks

Harsha

3 Replies

2,704 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Harsha Ganegoda,

There are many debuggers you can use , for example Segger J-link, SEGGER - The Embedded Experts - Downloads - J-Link / J-Trace   Universal Multilink FX  Universal Multilink FX High-Speed Development Interface|NXP or others .

" If I buy FRDM-KL26Z development platform can I use it as a programmer?"

-> Yes, you can use the debugger(OpenSDA) on FRDM-KL26 debug other boards, about the method, please  refer to: Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards | MCU on Eclipse  

Hope it helps,


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,705 Views
hb0038
Contributor II

Hi Alice_Yang,

Thank you so much. But those debuggers are expensive so that's why I thought to use FRDM board and program via OpenSDA. So I bought FRDM-KL25Z board and tried to program my custom board which has NXP KL24Z processor. I used MCUXpresso IDE to program it. But I was not able to program my board using OpenSDA. :smileysad:
I used MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.SDA firmware. I could not find firmware for KL24Z processor. 

0 Kudos
Reply

2,705 Views
BlackNight
NXP Employee
NXP Employee

Hi Harsha,

you only can program the same microcontroller using the MSD programming mode (see Using the Freedom Board as SWD Programmer | MCU on Eclipse  for details), because the MSD programmer is specific to the device on the board. About programmers to be expensive: there is the J-Link EDU (mini) for $20 or the LPC-Link2 which you can use with MCUXpresso IDE to program any LPC *and* Kinetis, see Custom 3D Printed Enclosure for NXP LPC-Link2 Debug Probes | MCU on Eclipse  for $20. I think a $20 price point is not 'expensive'?

I hope this helps,

Erich

0 Kudos
Reply