ProcessorExpert and KDS project file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ProcessorExpert and KDS project file

1,052 次查看
oaf
Contributor IV

Hi,

 

There is one issue regarding PEx and KDS which is quite annoying.

1. The PEx doesn't delete generated files from Beans removed from the project

2. The KDS project file compiles *.c

The net effect is that a PEx module which is removed, will be compiled with your project and may cause some

unwanted behaviour. Working one person may go right, if you are careful, but working in a multi-people project

will cause trouble.

I would like to have some kind of fix for this problem....

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

986 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Ole,

can you please check if this properties setting can help you:

2015-05-27_12-13-35.png

if can't help, please specify more about your problem, I will check it further. thanks!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复