ProcessorExpert and KDS project file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ProcessorExpert and KDS project file

1,119件の閲覧回数
oaf
Contributor IV

Hi,

 

There is one issue regarding PEx and KDS which is quite annoying.

1. The PEx doesn't delete generated files from Beans removed from the project

2. The KDS project file compiles *.c

The net effect is that a PEx module which is removed, will be compiled with your project and may cause some

unwanted behaviour. Working one person may go right, if you are careful, but working in a multi-people project

will cause trouble.

I would like to have some kind of fix for this problem....

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,053件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hi Ole,

can you please check if this properties setting can help you:

2015-05-27_12-13-35.png

if can't help, please specify more about your problem, I will check it further. thanks!


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信