Processor Expert generate too much code as expected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert generate too much code as expected

ソリューションへジャンプ
1,803件の閲覧回数
gschelotto
Contributor V

Hello,

I'm using KDS v3.2 with KDSK 1.3 and PE. After creating a new project for FRDM-KL03Z I've initialized some PE components as spiCom1, gpio1... as shown in the next screenshot. Then I've just added a while(1) in main.c and the compilation result ends up in almost 14KB for the .text section that means a half of the total flash memory (32KB of the MKL03Z32VFK4).

166047_166047.pngUntitled.png

Can anybody help me to reduce the generated/compiled code? I find it too much for a few components initialization.

Here I attach the whole project for better understanding.

regards,

gaston

Original Attachment has been moved to: testing.zip

ラベル(1)
0 件の賞賛
返信
1 解決策
1,645件の閲覧回数
therealfreegeek
Contributor IV

The problem is less to do with PE and more to do with the KSDK components which are large, this is compounded by  KSDK's usage of ‘assert()’ in the driver code which uses the PRINTF function call which is huge.

Have a look at this https://mcuoneclipse.com/2016/03/09/dealing-with-code-size-in-kinetis-sdk-v2-x-projects/ it refers to KSDK 2 but I guess it is also relevant for 1.3.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,646件の閲覧回数
therealfreegeek
Contributor IV

The problem is less to do with PE and more to do with the KSDK components which are large, this is compounded by  KSDK's usage of ‘assert()’ in the driver code which uses the PRINTF function call which is huge.

Have a look at this https://mcuoneclipse.com/2016/03/09/dealing-with-code-size-in-kinetis-sdk-v2-x-projects/ it refers to KSDK 2 but I guess it is also relevant for 1.3.

0 件の賞賛
返信