Processor Expert Driver Suite 10.4 Update 1 applicable to KDS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert Driver Suite 10.4 Update 1 applicable to KDS?

Jump to solution
1,629 Views
DavidBLit
Contributor II

Greetings,

 

Not knowing the tribal lore and other accursed arcana of KDS, CodeWorrier, Eclipse, PE, PE Driver Suite, blah, blah, blah I can't tell if this update thing:

 

Processor Expert Software

 

...is something that should be installed if I currently have only KDS.

 

Should I:

 

- install it?

- not install it?

- long for the days of simple clarity?

- start drinking?

- ?

 

 

Thanks,

Dave

Labels (1)
0 Kudos
Reply
1 Solution
1,435 Views
BlackNight
NXP Employee
NXP Employee

Hi Dave,

this is an Update for the Driver Suite (the standalone Processor Expert version, or if you have added Processor Expert to your own Eclipse version).

There are dedicated upates for Processor Expert integrated into a tool chain like CodeWarrior or KDS. So this update does not apply to KDS.

You will get the 10.4.1 functionality integrated with the release of KDS V1.1 scheduled first week of August.

Regards,

Erich

View solution in original post

0 Kudos
Reply
1 Reply
1,436 Views
BlackNight
NXP Employee
NXP Employee

Hi Dave,

this is an Update for the Driver Suite (the standalone Processor Expert version, or if you have added Processor Expert to your own Eclipse version).

There are dedicated upates for Processor Expert integrated into a tool chain like CodeWarrior or KDS. So this update does not apply to KDS.

You will get the 10.4.1 functionality integrated with the release of KDS V1.1 scheduled first week of August.

Regards,

Erich

0 Kudos
Reply