Processor Expert Driver Suite 10.4 Update 1 applicable to KDS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert Driver Suite 10.4 Update 1 applicable to KDS?

ソリューションへジャンプ
1,630件の閲覧回数
DavidBLit
Contributor II

Greetings,

 

Not knowing the tribal lore and other accursed arcana of KDS, CodeWorrier, Eclipse, PE, PE Driver Suite, blah, blah, blah I can't tell if this update thing:

 

Processor Expert Software

 

...is something that should be installed if I currently have only KDS.

 

Should I:

 

- install it?

- not install it?

- long for the days of simple clarity?

- start drinking?

- ?

 

 

Thanks,

Dave

ラベル(1)
0 件の賞賛
返信
1 解決策
1,436件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Dave,

this is an Update for the Driver Suite (the standalone Processor Expert version, or if you have added Processor Expert to your own Eclipse version).

There are dedicated upates for Processor Expert integrated into a tool chain like CodeWarrior or KDS. So this update does not apply to KDS.

You will get the 10.4.1 functionality integrated with the release of KDS V1.1 scheduled first week of August.

Regards,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,437件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Dave,

this is an Update for the Driver Suite (the standalone Processor Expert version, or if you have added Processor Expert to your own Eclipse version).

There are dedicated upates for Processor Expert integrated into a tool chain like CodeWarrior or KDS. So this update does not apply to KDS.

You will get the 10.4.1 functionality integrated with the release of KDS V1.1 scheduled first week of August.

Regards,

Erich

0 件の賞賛
返信