Processor Expert Asynchronous Serial Race Condition?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert Asynchronous Serial Race Condition?

ソリューションへジャンプ
1,803件の閲覧回数
markwyman
Contributor III

Again I am running into nuisance problems in Processor Expert. This time I am running into problems with the Serial_LDD on the MKV31F512VLL12 processor. 

 

I have events for OnBlockReceived, OnBlockSent, and OnTxComplete all turned on. In each of these interrupts I have a volatile flag set to TRUE when these events complete.

 

The problem is when I make multiple calls to the following routine:

/************************************************
 * Send a string to the console. If entering here
 * before send is complete, this will block until
 * previous send has completed.
 */
void AS1_SendString(char *null_term_string)
{
 uint16_t len;

 if (mySerialPtr == NULL) return;

 len = strlen(null_term_string);
 //Cap length, these are strings after all, not full data.
 if (len > MAX_SEND_STRING_LEN) len = MAX_SEND_STRING_LEN;

 //Wait for previous send to fully complete.
 while(globals.AS1_TXComplete == FALSE)
 {
 }

 Error = ERR_BUSY;
 //Wait for all bytes to be put into the queue.
 while (Error == ERR_BUSY)
 {
 //Wait until completely sent to begin another.
 Error = AS1_SendBlock(mySerialPtr, null_term_string, len);
 //Flag that new block has not yet been sent.
 globals.AS1_DataSent = FALSE;
 globals.AS1_TXComplete = FALSE;
 }
}

It trashes the completion of the previous send, the last byte in the previous send gets aborted. It wold be the assumption that the OnTxComplete() interrupt should fire after the last bit goes out hardware-wise, and then the AS1_SendBlock() will also not report busy, but it appears the interrupt for AS1_OnTxComplete() fires at the start of the last byte transmission, and then the call to AS1_SendBlock() thinks all is ready (as there are no bytes left in the buffer), and the next send setup trashes the last byte currently in-progress.

 

I am able to add a delay and make it work in order to allow that last byte to complete, but of course that is certainly not ideal on a high-performance DSC as the less blocking, the better.

 

Any suggestions on a work-around to prevent needing to spin a delay in this code? I am trying to dump data arrays to a console for analysis, and getting lost characters. I suppose I could set up a massive buffer and dump the whole thing at once and avoid the problem, but I would like to get to the bottom of this one.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,609件の閲覧回数
markwyman
Contributor III

I did find the issue. It was me. I was not copying over the data I wished to send into a separate buffer before sending, but instead sending the buffer I was actively modifying directly. This led me to some odd conclusions, but obviously not the right ones! I made the erroneous assumption that the SendBlock() provided buffering for me.

I have been doing hardware design and board layouts too long, I guess I am a bit rusty.

Sorry about the false alert.

Corrected:

/************************************************
 * Send a string to the console. If entering here
 * before send is complete, this will block until
 * previous send has completed.
 */
void AS1_SendString(char *null_term_string)
{
 uint16_t len;

 //If driver not yet setup, exit.
 if (mySerialPtr == NULL) return;

 //Wait until prior send is complete before over-writing the buffer.
 while (globals.AS1_TXComplete == FALSE)
 {
 }

 //Copy just the bytes we wish to send, len ends with count of bytes.
 for (len = 0; (len < MAX_SEND_STRING_LEN) && (null_term_string[len] != 0x00); len++)
 {
 uart_outp_data[len] = null_term_string[len];
 }

 //Send the data...
 Error = AS1_SendBlock(mySerialPtr, uart_outp_data, len);
 globals.AS1_TXComplete = FALSE;
}

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,609件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mark,

Sorry i can not clearly know the problem.

Could you please tell me what function you want to realize , and you can

also send your project to me , then we can refer to it to analyze your question .

BR

Alice

0 件の賞賛
返信
1,610件の閲覧回数
markwyman
Contributor III

I did find the issue. It was me. I was not copying over the data I wished to send into a separate buffer before sending, but instead sending the buffer I was actively modifying directly. This led me to some odd conclusions, but obviously not the right ones! I made the erroneous assumption that the SendBlock() provided buffering for me.

I have been doing hardware design and board layouts too long, I guess I am a bit rusty.

Sorry about the false alert.

Corrected:

/************************************************
 * Send a string to the console. If entering here
 * before send is complete, this will block until
 * previous send has completed.
 */
void AS1_SendString(char *null_term_string)
{
 uint16_t len;

 //If driver not yet setup, exit.
 if (mySerialPtr == NULL) return;

 //Wait until prior send is complete before over-writing the buffer.
 while (globals.AS1_TXComplete == FALSE)
 {
 }

 //Copy just the bytes we wish to send, len ends with count of bytes.
 for (len = 0; (len < MAX_SEND_STRING_LEN) && (null_term_string[len] != 0x00); len++)
 {
 uart_outp_data[len] = null_term_string[len];
 }

 //Send the data...
 Error = AS1_SendBlock(mySerialPtr, uart_outp_data, len);
 globals.AS1_TXComplete = FALSE;
}

0 件の賞賛
返信